跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

PFO is selected by FSR, is the value set on the Port Pi Register output?

Latest Updated:02/14/2006

Question:

When Peripheral Function Output is selected by Function Select Register, is the value set on the Port Pi Register output?

Answer:

When using peripheral functions, the value set on the Port Pi Register is not output.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80