跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

On the H8S/2345 will /CS0 pin be Low during internal ROM access ?

Latest Updated:03/18/2009

Question:

On the H8S/2345 will /CS0 pin be Low during internal ROM access ?

Answer:

The /CS0 pin is not LOW during the ROM access. It is Low only when area 0 is accessed as external space.
Suitable Products
H8S Family
  • 这篇文章对您有帮助吗?