跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is there any way to detect a break signal sent from terminal side?

Latest Updated: 03/20/2017

Question:

Is there a way to detect a break signal (180 to 250ms mark state) sent from the terminal side when starting asynchronous serial communication?

Answer:

If the PM register of the corresponding port is set to input, the status of the RXD0 to RXD2 pins can be read as a port.
Suitable Products
V850 Family