跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is there a version of the H8/3664 with on-chip EEPROM ?

Latest Updated:03/18/2009

Question:

Is there a version of the H8/3664 with on-chip EEPROM ?

Answer:

The H8/3664N is a pin and function compatible version of the H8/3664F but offers an additional 512 bytes of EEPROM. Renesas uses its MCP ( Multi-Chip Packaging ) technology to place two die the H8/3664F die and a 512 byte I2C EEPROM die in one package.
Suitable Products
H8/300H Tiny