跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is the same oscillation circuit used for on-chip EEPROM products?

Latest Updated:03/26/2009

Question:

Is the same oscillation circuit for reference use recommenced for on-chip EEPROM products?

Answer:

The same circuit is used for them, because HD64F3664FP and HD64N3664FP respectively use the same chip.
Suitable Products
H8/300H Tiny
H8/3694
H8/3687
H8/3664