跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does a new interrupt request keep until the current interrupt is completed?

Last Updated:12/26/2017

Question:

If a new interrupt request is generated while already servicing the same interrupt, is this new interrupt request retained until the current interrupt service routine is completed?

Answer:

The interrupt request bit(IR bit) goes to "1" when an interrupt request is generated and to "0" automatically when the program branches to the interrupt routine. If another interrupt request caused by the same source is generated, after the program has branched to the interrupt routine and the IR bit has changed to "1", the new interrupt request will be retained. However, if another interrupt request caused by the same source is generated while the IR bit is still "1", IR will not be retained.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC