跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it possible to use the reserved area of ROM?

Latest Updated:09/29/2006

Question:

(ROM)  The datasheet and user's manual state that the first 128 bytes and the last 2 bytes of ROM are reserved for product testing, and the rest is user area. Can the reserved area be used? [2006/09/29]

Answer:

  1. Flash Memory version
    The reserved areas can be used.
  2. QzROM version and Mask ROM version
    Please do not use the reserved area.

Supplemental note:
When the QzROM version or Mask ROM version are mass produced, user programs cannot be written into the reserved area because the area is occupied by testing programs. Care should be taken when switching from Flash Memory version to Mask ROM version or QzROM version.

(#105523)

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549