跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is it okay to input valid waveforms to pins that are set for key on wake up?

Latest Updated:07/04/2003

Question:

(Power Save)  In modes other than power down mode, is it okay to input valid waveforms to pins that are always set for the key-on wakeup function?

Answer:

No problem. The key-on wakeup function is enabled only in power down mode. (#105024)
Suitable Products
4559
455A