跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

In memory expansion mode, how do I use UART6 or UART7?

Latest Updated:02/24/2012

Question:

In memory expansion mode, how do I use UART6 or UART7?

Answer:

In memory expansion mode and microprocessor mode, UART6 and UART7 cannot be used, even if an 8-bit data bus is used (D6 to D15 not used) or the output from CS2/CS3 is disabled.
Suitable Products
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C