跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

I2C Special Mode Interrupts and Exit Wait/Stop Mode

Last Updated:08/24/2017

Question:

In the User's Manual: Hardware, it states that the I2C serial interface interrupts can used be for exit wait/stop mode.  Are these interrupts available in any of the modes?

Answer:

The start/stop condition detection interrupt for Special Mode 1 of the I2C of the serial interface (UARTi) cannot be used to exit wait/stop mode.
Suitable Products
M16C Family (R32C/M32C/M16C)