跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to treat COM4 pin if the LCD driver of Super Low used with 1/3 duty?

Latest Updated:03/18/2009

Question:

I'd like to know how to treat COM4 pin when the LCD controller driver of Super Low Power Series is used with 1/3 duty.

Answer:

Please leave the COM4 pin open circuit.
Suitable Products
H8 Family
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8/300L
H8 Super Low Power