跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How to program FDT and E8 to do some on board programming on the QzROM?

Latest Updated:07/31/2008

Question:

(QzROM, Programmers)  I am using a Flash Development Toolkit (FDT) and E8a to do some on-board programming on the QzROM version but am unable to program. Why? [2008/07/31]

Answer:

You need an IC Socket Board when on-board programming the QzROM version.
Connect an IC socket board between the E8a and user board.
Click here for more details. (#107063)
Suitable Products
3803H
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549
E8a
E8