跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How should I consider the conversion time in sweep mode*?

Latest Updated:06/23/2010

Question:

How should I consider the conversion time in sweep mode*?

Answer:

For the A/D converter of this product, it is not necessary to consider the time to switch the pins in sweep mode*.
The conversion time will be as follows:

[Conversion time] = [conversion time per pin] x [number of A/D sweep pins]

*Sweep mode: Indicates single sweep mode, repeat sweep mode 0, and repeat sweep mode 1.

Suitable Products
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A