跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How much is MCU's current consumption rises when using A/D converter?

Latest Updated:10/10/2008

Question:

(A/D Converter, Electrical Characteristics)  How much is the MCU's current consumption increased when using an A/D converter? [2008/10/10]

Answer:

Please refer to the following pages for figures of the A/D converter's current consumption characteristics. Click the Group name of your MCU.

Click:
3823   38D2   38D5    7542    7546    7547    7548    7549

Standard characteristics are example measurements of standard samples. They are provided for reference only and are not guaranteed.
For standard values, please refer to "Electrical Characteristics" in the datasheet for your device. (#107143)

Suitable Products
3803H
3823
3850A
38D2
38D5
7545
7546
7547
7548
7549