跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How do I suppress consumption current in stop mode and wait mode?

Latest Updated:09/21/2010

Question:

How do I suppress consumption current in stop mode and wait mode?

Answer:

The "Concept of the Power Control" application notes (MEJ05B0130) contains information on low power operation using wait mode and stop mode of the M16C Family. Please refer to it.
Suitable Products
M32C/95
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A