跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

How can I set the lock bit to "1" (unlock)?

Latest Updated:03/08/2012

Question:

How can I set the lock bit to "1" (unlock)?

Answer:

Perform an erase with the FMR02 bit set to "1" (block lock disable). After erasing, the lock bit will go to "1".
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P