跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

General registers as 8-bit, 16-bit, 32-bit registers at the same time

Latest Updated:03/26/2009

Question:

Can different general registers be used as 8-bit, 16-bit, and 32-bit registers at the same time?

Answer:

Yes. Registers can be set freely for use as follow.

Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902