跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does timer 2 and timer LC count starts timing when operation starts?

Latest Updated:01/17/2005

Question:

(Timer)   Timer 2 and timer LC count start timing and count time when operation starts. [2005/01/17]

Answer:

Count starts from the rising edge (2) after the first falling edge of the count source, after timer 2 and timer LC operations start (1).
Subject to the operation start timing of the timers and count source, after count starts, the time to the first underflow (3) will be different from the time between subsequent underflows (4). (#105078)

Suitable Products
4559
455A