跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does the program fetch to Bank 7 regardless of the bank selection?

Latest Updated:03/08/2012

Question:

The manual describes 4-Mbyte Mode(the memory space expansion mode 2) as "When 4-Mbyte Mode(the memory space expansion mode 2) is selected, the bank selection function allows the user to switch the address space." Does the program fetch go to Bank 7 (program area) regardless of the bank selection?

Answer:

The CPU accesses Bank 7 during the program fetch and there is no bank selection necessary for this access.
Suitable Products
M16C/62N
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C