跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Does M16C Flash Starter supports writing to 3803, 3804 and 3886?

Latest Updated:12/07/2004

Question:

(Flash Memory)   Does M16C Flash Starter (M3A-0806) support writing to 3803 (standard), 3804 (standard) and 3886? [2004/12/70]

Answer:

There are no plans to support this. (#104932)
Suitable Products
3803H
3803L
M3A-0806