跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Do files filed by M3T-ICC740, M3T-SRA74 support M16C Flash Starter?

Latest Updated:03/01/2005

Question:

(Flash Memory)   Do files compiled and generated by M3T-ICC740 and M3T-SRA74 support M16C Flash Starter (M3A-0806)? [2005/03/01]

Answer:

Converting to the Motorola S2 format is needed in order to use files with M3A-0806. Use the "HEXTOS2" conversion software attached to the M3A-0806 execution file to convert the file format. Refer here for more on M3A-0806. (#104964)
Suitable Products
3850A
38D2
38D5
M3A-0806