跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can you choose key-on wake up to be valid or invalid for each pin?

Latest Updated:03/22/2012

Question:

Is it possible to select whether key-on wake up is valid or invalid for each pin?

Answer:

Yes, it is possible.
The key-on wake up function is disabled for pins that are set to output mode using the port direction register.
Suitable Products
M16C/62A
M16C/62N
M16C/62P
M16C/63
M16C/64
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A