跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can the whole user ROM area be used even if it overlaps the boot ROM area?

Latest Updated:10/10/2006

Question:

The addresses of the user ROM area and boot ROM area overlap, however, can the whole user ROM area be used?

Answer:

The user ROM area and boot ROM area are located in different spaces so the whole user ROM area can be used. Please refer to the chapter of "Usage notes for on-chip debugger" in the hardware manual to use an on-chip debugger.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L