跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can the clock output pin CLKOUT be used in memory expansion mode?

Latest Updated:03/15/2012

Question:

Can the clock output pin CLKOUT be used in memory expansion mode? Or, is there any equivalent function available?

Answer:

The P57/RDY/CLKOUT pin functions as RDY input pin in the memory expansion or microprocessor modes. That is why you cannot use it as clock output pin. Please use the BCLK pin or the Timer A output pins in the memory expansion and microprocessor modes.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/30P