Can PWM output be set to start at "H" level?
Latest Updated:03/01/2005
Question:
(PWM Output) Can PWM output be set to start at "H" level? [2005/03]
Answer:
After PWM is enabled using the PWM function enable bits, PWM output will start from "H" after a brief "L" level output from the respective PWM pin. "L" level output duration is as follows:
- When the count source selection bit = "0"
(n + 1)/(2×f(XIN)) seconds n = value set in the PWM prescaler
- When the count source selection bit = "1"
(n + 1)/f(XIN)) seconds n = value set in the PWM prescaler
(#104811)
Suitable Products
3803H |
3803L |
3850A |
3858 |