跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I use the interrupt nesting?

Latest Updated:10/10/2006

Question:

Can I use the interrupt nesting?

Answer:

Yes.
Set the interrupt flag(I flag) to "1" in the interrupt routine. The interrupt with the higher priority than the processor interrupt request(IPL) at the time is accepted.(The interrupt request with the same priority as IPL isn't accepted.)
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC