跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I leave the BCLK pin open when the BCLK output is disabled?

Latest Updated:03/15/2012

Question:

The user's manual describes that when the BCLK output is disabled in the memory expansion mode, the BCLK pin goes to the floating state. On the other hand, the manual indicates that the BCLK pin can be opened when the pin is not used. Can I leave the BCLK pin open when the BCLK output is disabled?

Answer:

Pull-up the BCLK pin through resistors when you disable the BCLK output. The pin open connection described in the manual is a solution example when the BCLK output is enabled and the BCLK pin is not used. When you enable the BCLK output, you can leave the pin open.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P