跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Can I connect the I/O port to the power supply directly when pulling up?

Latest Updated:03/25/2009

Question:

Can I connect the I/O port to the power supply directly when pulling up?

Answer:

A pull-up resister is required. Please refer to electrical characteristics for the resistance value.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902