跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Block erase time standard and maximum values

Latest Updated:10/05/2016

Question:

Regarding the standard value shown for block erase time under flash memory electrical characteristics, when both a standard and maximum value are shown, what are the conditions for approaching the maximum value?

Answer:

As the number of program/erase endurance increases, the block erase time tends to lengthen.
Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/33T
R8C/3JT
R8C/3NT
R8C/36T-A
R8C/38T-A
R8C/3MK
R8C/34K
R8C/3MU
R8C/34U
R8C/3MQ
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
R8C/LA3A
R8C/LA5A
R8C/LA6A
R8C/LA8A
R8C/Mx
  • 这篇文章对您有帮助吗?