跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Are there sample program for receiving infrared signals in NEC format?

Latest Updated:04/01/2006

Question:

Are there any sample programs for receiving infrared remote control signals in NEC format?

Answer:

For sample programs, consult an NEC Electronics sales representative.

Also refer to the following FAQ item for reception processing: NEC format for infrared remote control [Common]
Suitable Products