跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

After the power on reset, what is the value of internal registers?

Latest Updated:03/25/2009

Question:

After the power on reset, what is the value of internal registers?

Answer:

"(1) On-chip I/O register are set to the initial value (There are exceptions for some cases. For more information, please refer to the hardware manual.)

(2) CPU register: PC is loaded from vector table, I bit = 1 in CCR, others such as from R0 to R7 and CCR are undefined."

Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902