跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(M16C/1,M16C/2,M16C/62P) What happens to count source when CPU clock is changed?

Latest Updated:02/27/2012

Question:

When a CPU clock is changed from a main clock to an on-chip oscillator clock, what happens to the count source of the peripheral function?

Answer:

The on-chip oscillator clock becomes the count source of the peripheral function.
However, the count sources of peripheral functions that were set to fC32 will be unchanged.
Suitable Products
M16C/62P
M16C/29
M16C/28
M16C/26A
M16C/1N