跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(4508) In the QzROM, can additional programs be written to the free area in ROM?

Latest Updated:05/24/2007

Question:

(QzROM)  In the QzROM version, can additional programs be written to the free area in ROM? [2007/05/24]

Answer:

As long as protection is not enabled, it is possible to write to the ROM. (#106674)
Suitable Products
4286
4508
4509
4559
455A
4571