跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(3850A) Are latch and timer written to during write in and timer value read out?

Latest Updated:03/01/2005

Question:

(Timer)   Are the latch and the timer simultaneously written to during write-in and the timer value read during read-out regardless of whether the timer is in operation or suspended? [2005/03/01]

Answer:

The timer and timer latch are written to simultaneously, and the timer count value is read-out.
(This is described in the register description in the "register list" in the user's manual.)
(#104785)
Suitable Products
3850A