跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why does the product that I want to use is not participating in PLP?

Latest Updated:04/01/2015

Question:

The product that I want to use is not participating in the Product Longevity Program (PLP). Why?

Answer:

Products that do not meet the conditions to be a PLP product (FAQ No. 1010888) do not participate in the program. Newly released products may also not have been added the to PLP yet. If you have any questions, please contact a Renesas sales office or representative.
Suitable Products
PLP (Product Longevity Program)