跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why do prebaking differ among products and some don't need prebaking?

Latest Updated:04/01/2006

Question:

Why do the prebaking conditions differ among products? And why do some products not require prebaking?

Answer:

Different products have different packages and internal chip sizes, so the vulnerability of moisture absorption and cracking differs depending on these factors.
Suitable Products