跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Why are Automotive products not included in the program?

Latest Updated:04/01/2015

Question:

Why are Automotive products not included in the program?

Answer:

Products for automotive applications are designed/developed on the premise of providing long product life cycles. Also, in most cases automotive customers have a individual contract and are receiving information about supply period individually. If a blanket estimated supply period were to be provided on the website for each automotive product, this would cause misunderstanding with customers. Thus, we determined that it would not be appropriate to include automotive products in the PLP.
Suitable Products
PLP (Product Longevity Program)