跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What is the difference between PLP products and non-PLP products?

Latest Updated:04/01/2015

Question:

What is the difference between PLP products and non-PLP products?

Answer:

For non-PLP products, transition to the EOL (end of life) phase is based on demand and other factors. PLP products are specially managed in a Renesas internal production management system and as a general rule cannot enter the EOL phase.
Suitable Products
PLP (Product Longevity Program)