跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Is participation in the Product Longevity Program set by part name?

Latest Updated:04/01/2015

Question:

Is participation in the Product Longevity Program (PLP) set by part name?

Answer:

In addition to the part names that are shown in datasheets, Renesas has orderable part numbers that a customer uses when placing an order. There can be several orderable part numbers for one part name, as orderable part numbers are created based on differences in materials, manufacturing facilities or other conditions. The PLP period is set for an orderable part number. Thus, a part name could have a mixture of PLP orderable part numbers and non-PLP orderable part numbers.
Suitable Products
PLP (Product Longevity Program)