跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

uPD780076中有象"EGP"和"EGN"这样以位为单元的特殊寄存器,但当用汇编程序处理这些寄存器时会有错误发生。

最新更新:2011年10月 06日

Question:

uPD780076中有象"EGP"和"EGN"这样特殊的以位为单元的寄存器,但是当我尝试用汇编程序处理这些寄存器的时候就会有错误发生。

Answer:

这款设备的用户手册的介绍中作过这样的解释,那些包括在内的位操作的寄存器才适用于RA78K0, 而没有包括在内的位操作寄存器就不适用于RA78K0。

如果用户想参考这些未定义的位,可以像"EGP.0"这样规定这些位编号。
参考文献:
RA78K0 Assembler Package -- Language
Suitable Products
 
  • 这篇文章对您有帮助吗?