跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

MPU/MCUPeripherals; 观察78K/0库管理程序中信息时会输出错误。为何会产生这些错误,该如何处理?

最新更新:2011年10月 06日

Question:

当我试图观察78K/0库管理程序中信息的时候,就会输出以下这些错误提示。
请问为什么会产生这些错误,我如何处理这些错误?

 
|   78K/0 Series Librarian V3.10  [ 5 Mar 96]
|      Copyright (C) NEC Corporation 1990,1996
|   *l cl0.lib
|   F104 Illegal library file - different target chip (file : CL0.LIB)
|   *

Answer:

之所以会输出这样的错误提示,是因为当创建cl0.lib的时候没有找到合适的设备文件。
你可以将uPD78014的设备文件包含进去试试。
uPD78014的设备文件可以在NEC网页中"Download Development Tools"处下载。

Suitable Products