跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

uPD789166数据手册描述了N-ch开漏输出和一个5V耐压输入缓冲器和13-X类型的比较器;但无比较器的描述。

最新更新:2011年10月 05日

Question:

uPD789166数据手册中,有一个关于引脚I/O电路的描述,并且描述了一个N-ch开漏输出,和一个5V耐压输入缓冲器和13-X类型的比较器;但是没有关于比较器的描述。

Answer:

这个比较器仅用于uPD789166Y的SMB接口,来检查SMB输入信号是否超过极限。
uPD789166没有SMB接口。uPD789166中没有提供比较器,请忽略。
顺便提一下,这个信息在数据手册中的5-10有描述。

Suitable Products