跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

uPD780024中若想在2线串行通讯模式下用SIO31作为只发不收的方式,SIO31发送模式中将PM34置为0即可?

最新更新:2011年10月 06日

Question:

在uPD780024中,我想在2线串行通讯模式下使用SIO31作为只发送不接收的方式工作,并设置SI31引脚为输出端口。
是否在SIO31发送模式中简单地将PM34设置为0就可以了?

Answer:

是的。
因为没有针对SIO31的只发送模式,那么通过简单地设置SIO31为发送/接收模式, 并将PM34设置为0(将端口34设置为输出模式),而使SI31引脚用作输出端口。
因为SIO31在传送期间接收的是无意义的数据,所以完全可以忽略接收到的数据。
Suitable Products