跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(PWM输出) 如何设定PWM输出为“L”?

最新更新:03/01/2005

Question:

(PWM输出) 如何设定PWM输出为“L”?

Answer:

有两种方法:
- 在当前PWM周期输出后输出“L”时,向PWM寄存器写“00h”,“L”电平输出从下一个PWM周期开始。

- 不等PWM周期结束就想立即输出“L",设定与PWM输出复用的引脚输出值为”0“,对应方向寄存器为”1“,
并且PWM功能使能位设为”0“(禁止)。将立即输出"L”电平。当按照上述端口初始设定后还使用PWM功能,
设定PWM功能使能位设为”1“将从下一周期开始切换输出“L"电平。

Suitable Products
3803H
3803L
3850A
3858