跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(LCD) What is the difference between "A type" and "B type" LCD drive timing ? [2004/10/19]

最新更新:10/19/2004

Question:

(LCD)  What is the difference between "A type" and "B type" LCD drive timing ? [2004/10/19]

Answer:

A type is equivalent to existing Renesas products.
B type can support LCD panels of slow responsivity.
Please select which type to use according to your LCD panel. (#104921)
Suitable Products
38D2