跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(Interrupt) Can ports P10 to P15 (P10 to P17 for 7549) be set to input mode and key-on wakeup enabled only for input to P10? [2008/03/13]

最新更新:03/13/2008

Question:

(Interrupt)  Can ports P10 to P15 (P10 to P17 for 7549) be set to input mode and key-on wakeup enabled only for input to P10? [2008/03/13]

Answer:

Yes.
Key-on wake up settings for each individual pin can be enabled and disabled using the key input control register. (#106882)
Suitable Products
7548
7549