跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(I/O端口,中断,LCD)不用LCD升压电路时如何处理P70/C1/INT01和P71/C2/INT11引脚?

最新更新:10/26/2006

Question:

(I/O 端口, 中断, LCD) 不使用LCD升压电路时,如何处理P70/C1/INT01 和P71/C2/INT11引脚?

Answer:

如果未使用引脚P70/INT01 或 P71/INT11,通过电阻将其连接至VSS并禁止升压电路(升压电路设定为“0”),建议循环写入该位,以防止故障;同时,如果使用引脚P70/INT01和 P71/INT11,也建议禁止升压电路并循环写入该位,以防止故障。
Suitable Products
38D5