跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(D/A转换器) DAI输出允许位为“0”(禁止)时,DAI引脚的状态如何?

最新更新:03/01/2005

Question:

(D/A转换器) DAI输出允许位为“0”(禁止)时,DAI引脚的状态如何?

Answer:

DAI输出允许位为“0”(禁止)时,DAI引脚功能与输入/输出端口共享,其状态由端口方向寄存器决定。端口方向寄存器的对应位为“0”时,该引脚设定为输入模式,处于高抗阻状态,当该引脚方向寄存器的相应位为“1”时,设定到输出模式,输出端口锁存的内容。
Suitable Products
3803H
3803L