跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(D/A转换器) 使用D/A转换器时,DAI引脚应设定为输入模式,是否可设定为输出模式?

最新更新:03/01/2005

Question:

(D/A转换器) 使用D/A转换器时,DAI引脚应设定为输入模式,是否可设定为输出模式?

Answer:

不可以,使用D/A转换器时,DAI引脚必须设定到输入模式(设定端口方向寄存器相应的位为“0”)。若端口设定为输出模式,端口输出电平和D/A转换器输出将发生内部冲突。因此,必须将方向寄存器设定为输入模式,然后设定DAI输出允许位为“1”(允许)。
Suitable Products
3803H
3803L