跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(闪存) M3T-ICC740和M3T-SRA74编译产生的文件是否支持M16C闪存启动工具(M3A-0806)?

最新更新:03/01/2005

Question:

(闪存) M3T-ICC740和M3T-SRA74编译产生的文件是否支持M16C闪存启动工具(M3A-0806)?

Answer:

为了使用M3A-0806工具,需要将文件转换为Motorola S2 格式。
请使用M3A-0806工具中的 "HEXTOS2"转换软件来转换文件格式,关于M3A-0806更多的信息请参考 这里
Suitable Products
3850A
38D2
38D5
M3A-0806